2019-08-26 8:38 AM
Hello,
with version STMCubeIDE 1.0.2, I get an 'unhandled event loop exception' after I've created a project and atttempt to look at the source code that is generated.
Effectively, this renders the IDE unusable, as the only option I have is to quit, as this errors keeps repeating itself.
It is hard to find out what is causing this bug, as the popup window is the only thing I can click in...
any ideas?
I'm using Ubuntu 18.04 to run this on and installed from the debian package for 1.0.2.
These errors started occuring after I updated from 16.04 to 18.04. But I reinstalled the STMCubeIDE...
2019-08-27 5:05 AM
Some more detailed info when starting from the command line; the error messages are repeating numerous times, but I cut them here for brevity.
***WARNING: Detected: GTK_IM_MODULE=xim. This input method is unsupported and can cause graphical issues.
***WARNING: Unset GTK_IM_MODULE or set GTK_IM_MODULE=ibus if flicking is experienced.
(STM32CubeIDE:9022): GLib-CRITICAL **: 14:01:52.225: g_base64_encode_step: assertion 'in != NULL' failed
(STM32CubeIDE:9022): Gtk-CRITICAL **: 14:02:25.858: gtk_box_gadget_distribute: assertion 'size >= 0' failed in GtkScrollbar
(STM32CubeIDE:9022): Gdk-CRITICAL **: 14:02:28.017: The window 0x7f75de488af0 already has a drawing context. You cannot call gdk_window_begin_draw_frame() without calling gdk_window_end_draw_frame() first.
2019-08-27 5:08 AM
Doing
export GTK_IM_MODULE="ibus"before starting stmcubeide seems to fix it...
though a lot of the error messages still happen. (the encode step and the scrollbar one)
2020-06-20 8:14 PM
I have been having the same Unhandled event loop exception problems. I'm running Debian 9, and getting rid of it, has been a real pain. Its related to the input ibus=xim bug
Here is a link talking about linux input handling . https://unix.stackexchange.com/questions/260601/understanding-setting-up-different-input-methods
Test with eclipse Version: 2020-06 (4.16.0) Build id: 20200615-1200 to see the problem.
It warns you about input , GTK_IM_MODULE="xim" being set, on startup (run from bash to see this startup warning)
you can use, im-config to change it, (install if you don't have ) to something else, but this dose not fix the problem!, X startup being complete abomination. It could being set in any number of other places. I removed ibus, nope, still get the warning from eclipse and the buffer flashing problem, and grep-ing all my config file's for gnome/gtk/X.. nop.. still could not find where it was being set, best I could come up with was to add this to .profile and .bash files
export GTK_IM_MODULE="gtk-im-context-simple"
export QT_IM_MODULE="simple"
This fix the problem for the moment(for me) but who knows, given the Java/Eclipse version nightmare, it may all stop working just by clicking the left mouse button at the same time your holding the Num lock key down, format your hard-disk, sign you up for a million $ loan at 200% interest , with your local shark loan organization, and then say.. Have a nice day!
Lachlan
2020-06-20 10:28 PM
Not quite there, fixed the flashing window problem but not the crash Unhandled event loop exception
so change my version of have Java to oracle.com 1.8.0_251 . (version) Note ST ships it's own version of java, which apear's to be openjdk version "1.8.0_242"
as STMCubeIDE looks for it's own version not the system version you will have ln -s to the new version of java, ST version is at /opt/st/stm32cubeide_1.3.0/jre/
for now it's working.. touch wood(my head!) LOL
Lachlan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.