2024-11-30 9:28 PM
I'm trying to access the external flash on a B-U585I-IOT02A. The driver(s) I found do:
if (HAL_SPIEx_SetConfigAutonomousMode(&hspi2, &HAL_SPI_AutonomousMode_Cfg_Struct) != HAL_OK)
but the linker says that function is undefined. Is that in a library file I haven't included (and haven't located to include it)?
-Marty
Solved! Go to Solution.
2024-12-01 10:49 AM - edited 2024-12-01 11:12 AM
Hello @Marty ,
Ensure that the HAL library source code file path is defined In project settings -> C/C++ General -> Paths and Symbols -> Source Location.
So, check your Library paths in your project settings and try to add the missing files into the src and inc folders.
Ensure that stm32u5xx_hal_spi.c is included in your project and is being compiled.
Make sure to have #define HAL_SPI_MODULE_ENABLED inside stm32u5xx_hal_conf.h file.
2024-12-01 10:49 AM - edited 2024-12-01 11:12 AM
Hello @Marty ,
Ensure that the HAL library source code file path is defined In project settings -> C/C++ General -> Paths and Symbols -> Source Location.
So, check your Library paths in your project settings and try to add the missing files into the src and inc folders.
Ensure that stm32u5xx_hal_spi.c is included in your project and is being compiled.
Make sure to have #define HAL_SPI_MODULE_ENABLED inside stm32u5xx_hal_conf.h file.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.