2025-11-25 3:00 AM - edited 2025-11-25 3:02 AM
Hello,
I can not start STM32CubeIDE_2.0.0.
I have the following error:
D:\ProgramFiles\STMicroelectronics\STM32CubeIDE_2.0.0\STM32CubeIDE;;.
C:\Users\Mich\.swt\lib\win32\x86_64\swt-win32-4966r5.dll: La procedure specifiee est introuvable
Can't load library: C:\Users\Mich\.swt\lib\win32\x86_64\swt-win32.dll
Can't load library: C:\Users\Mich\.swt\lib\win32\x86_64\swt.dll
C:\Users\Mich\.swt\lib\win32\x86_64\swt-win32-4966r5.dll: La procedure specifiee est introuvable
In directory .swt\lib\win32\x86_64 there is only swt-win32-4966r5.dll file.
Why the installer does not put these files?
Do you have any correction please?
Best regards
Michel
Solved! Go to Solution.
2025-11-25 6:15 AM - edited 2025-11-25 6:17 AM
Hello @MLe M.1 ,
Related to STM32CubeIDE 2.0 Release Note:
Host PC system requirements
Supported operating systems and architectures
• Windows® 10 and 11, 64 bits (x64)
• Linux®: Ubuntu® LTS 22.04 and LTS 24.04, and Fedora® 42
• macOS® 15 (Sequoia), macOS® 26 (Tahoe)
Note: Windows is a trademark of the Microsoft group of companies.
Linux® is a registered trademark of Linus Torvalds.
Ubuntu® is a registered trademark of Canonical Ltd.
Fedora® is a trademark of Red Hat, Inc.
macOS® is a trademark of Apple Inc., registered in the U.S. and other countries and regions.
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-11-25 3:08 AM
You haven't said what Windows version you're using; also, 32 or 64 bit ?
How to write your question to maximize your chances to find a solution
2025-11-25 3:15 AM
Hello @MLe M.1 ,
Let me thank you for posting.
For more investigation, could you please provide the Operation System used.
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-11-25 6:12 AM
Windows 8.1 Professionnel
x64
2025-11-25 6:15 AM - edited 2025-11-25 6:17 AM
Hello @MLe M.1 ,
Related to STM32CubeIDE 2.0 Release Note:
Host PC system requirements
Supported operating systems and architectures
• Windows® 10 and 11, 64 bits (x64)
• Linux®: Ubuntu® LTS 22.04 and LTS 24.04, and Fedora® 42
• macOS® 15 (Sequoia), macOS® 26 (Tahoe)
Note: Windows is a trademark of the Microsoft group of companies.
Linux® is a registered trademark of Linus Torvalds.
Ubuntu® is a registered trademark of Canonical Ltd.
Fedora® is a trademark of Red Hat, Inc.
macOS® is a trademark of Apple Inc., registered in the U.S. and other countries and regions.
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-11-25 6:33 AM - edited 2025-11-25 6:36 AM
As @Mahmoud Ben Romdhane said, that's not supported - this is also stated in the User Manual:
PS:
Maybe take a look at What last version of STM32CubeProgrammer for Windows 7 supported? and work from there ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.