2020-08-22 1:07 AM
Hello everyone,
at first the Discoveryboard I'm using is the P-L496G-Cell02 / STM32L496G-DISC.
To test the ADC I tried to recieve a value from a potentiometer.
So I started a new STM32CuvbeIDE project, Selected the board I'm using and changed the Pins (via the CubeMX Interface) to the correct Input. I tried it several times with different pins:
PC4 -> ADC2_IN13
PC1-> ADC1_IN2
PC3-> ADC1_IN4
And i changed the associated channel to Single-ended.
In the main fuction, i declared a variable raw and added the code in the while-loop
int main(void)
{
uint16_t raw;
HAL_Init();
SystemClock_Config();
MX_ADC2_Init();
while (1)
{
/* USER CODE END WHILE */
HAL_ADC_Start(&hadc2);
HAL_ADC_PollForConversion(&hadc2, HAL_MAX_DELAY);
raw = HAL_ADC_GetValue(&hadc2);
HAL_Delay(2);
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}As a result raw is always 4095 (3.3V) even if i unplug the cable to the potentiometer.
I hope somebody can help me with this problem
2020-08-22 1:13 PM
2020-08-24 3:37 AM
Today I tried several things:
1.Changed the ADC2 regular Channel to 13 and got the same result.
sConfig.Channel = ADC_CHANNEL_13;2. Connected PC4 to the potentiometer ->4095
3. Connected PC4 to ground ->4095
4. Connected PC4 to 3.3V ->4095
5. Connecteed PC4 to ground with an resistor in between -> showing 0 and 4095 in irregular intervals
6. Generate the code with an older MX-Version 5.6.1 ->4095
7.Tried the code snippet I posted in the first post on an other discoveryboard (stm32f4) with the generated code from the CubeMX->Everything is working as it should
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.