2024-10-22 11:26 PM
Issue occurs in this build:
To reproduce:
The workaround is to edit the symbols elsewhere see below noting where I added the extra quote:
2024-10-22 11:42 PM
Hello @davef and welcome to the ST Community.
I'm sending this for internal investigation, and I will be back to you as soon as I have a clear answer.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-23 3:30 PM
Thank you. Another thing I noticed is that system environment variables only seem to be refreshed on opening the workspace, is there a way to refresh the cached environment variables when running a pre compile action or script?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.