2026-04-08 10:55 PM
Hi Support
I have experience in STM32 with Zephyr but I am trying out AMP for the first time.
So I am trying out OpenAMP example from STM32CubeIDE. I can compile the example but cannot flash the same.
I have the following error
The ST-Link device is present as shown below
I have tried other boards like NUCLEO-G431RE with some simple UART example and work well.
I have problems only with AMP board, I am not able to flash M4 and M7 core.
My dev environment
Ubuntu 22.04 and STM32CubeIDE ver1.1.8.1
Could anyone please help me understand the same?
Solved! Go to Solution.
2026-04-09 2:41 AM
This Board has also not worked with CubeProgrammer in Linux. I will try on Windows and will update again
2026-04-09 2:43 AM
@jo512 wrote:
This Board has also not worked with CubeProgrammer in Linux. I will try on Windows and will update again
Yes do it please ..
2026-04-09 3:03 AM
Has it ever work at all ?
What's it's history?
2026-04-09 3:17 AM
Hi Andrew,
This is a new board right out of the box. And has never worked in my hands
Regards
Jo
2026-04-09 3:43 AM
You need to ensure the connection step with CubeProgrammer.
You need to ensure the connection to each of the Cores CM4 and CM7:
To connect to CM7, you need to set the access port to 0:
To connect to CM4, you need to set the access port to 3:
Ensure also all the jumpers are set correctly especially JP6: it should be set to ST-LINK option.
If you succeed to connect with CubeProgrammer, try to update the ST-LINK firmware with CubeProgrammer:
Then,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.