2022-03-07 9:13 AM
2022-03-07 9:37 AM
Welcome, @MSpir.2, to the community!
For this application, there are amplifier circuits that turn a smaller voltage into a larger one. In your case, you would have to use a non-inverting amplifier with a gain factor of 5V/VDD (if VDD=3.3, then =5/3.3), which can be realised quite easily with a low-voltage opamp with RRIO pins (rail-to-rail input and output).
Does it answer your question?
Regards
/Peter
2022-03-15 6:25 AM
Do you need additional hints?
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.