2023-05-22 8:25 AM
Hello!
We are trying to add some header files to a project loaded in STM32CubeIDe.
We are setting new files path via this menu - “Project ! Properties ! C/C++ General ! Paths and Symbols ! Library Paths�?
Files are in specified directories but when we try to compile the project compiler couldn't find header files?!
Attached is the output from the compilation.
Would you please advice!
2023-06-01 7:40 AM - edited 2023-11-20 4:53 AM
Hello @Community member
First let me thank you for posting.
Could you check if the includes are well set in the "C/C++ Build/ Settings/ MCU GCC Compiler/ Includes paths"
KR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.