2023-05-25 7:18 AM
I am trying to flash an image into a target to debug. I am using STM32CubeIDE v1.12.0. I enabled logging when I start the debugger. The first error encounter is "Encountered Error when opening:\ST\STM32CubeIDE_1.12.0 . . . \STM32_Programmer_CLI.exe". I have verified the file exists and I can execute it manually. But the program exits so quickly I cannot determine if there is an error displayed. I know the target hardware is good because I can download and debug using older versions of STM32CubeIDE (1.8.0). Any suggestions would be much appreciated.
2023-06-01 7:37 AM
Hello @DCard.4
First let me thank you for posting.
Could you provide the complete debug log.
KR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-06-01 7:45 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.