STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Behaviour differences in STMCube32IDE when compiling without optimisation, failing to handle any functions declared as inline unless made static

There are still behaviour differences in the latest STMCube32IDE when compiling without optimisation O0, as it is failing to compile any functions declared as inline unless made static. Using O2 optimisation this does not happen and it compiles.Also ...

Robmar by Senior III
  • 1432 Views
  • 2 replies
  • 0 kudos

STM32ICubeDE Debugging fails on Windows 10 PC

I am getting an error trying to run the debugger for my project on my Windows 10 PC. It works on my Windows 7 PC (exact same project).An internal error occurred during: "Launching TERM_SERVER_F437_LWIP Debug".'com.st.stm32cube.ide.mcu.toolchain.IToo...

mvonahnen by Associate III
  • 2007 Views
  • 2 replies
  • 0 kudos

B-L475E-IOT01A2 - When using the XCUBE-BLE2 pack it seems that MCU hangs when the code resets the BLE module during initialization

Hello,I use the B-L475E-IOT01A2 board and I try to integrate/experiment with the BLE module.I created a new project using the STM32CubeIDE where I let the IDE apply the basic configuration for the board.Then I select the BLE2 pack which I configure t...

Software download issues

I can't download STM32CubeIDE although I got an dowload email from st. The button in the email works, but when I get on the STM32CubeIDE download page and click the download button, nothing happens.

HHumm.2 by Associate
  • 1145 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.