2022-11-21 12:04 PM
I just upgraded to MacOX Ventura 13.0.1 from MacOS 12 last night, and now STM32CubeIDE 1.10.1 crashes about 8 1/2 minutes from app startup, consistently. This is on a 2019 Intel 16" MacBook Pro. The crash happens even if the app is left idle.
Has anyone else experienced this? Any suggestions on how to fix this?
Here's part of the crash dump. I can post everything if needed.
-------------------------------------
Translated Report (Full Report Below)
-------------------------------------
Process: stm32cubeide [12688]
Path: /Applications/STM32CubeIDE.app/Contents/MacOS/STM32CubeIDE
Identifier: stm32cubeide
Version: ???
Code Type: X86-64 (Native)
Parent Process: launchd [1]
User ID: 502
Date/Time: 2022-11-21 11:54:25.8404 -0800
OS Version: macOS 13.0.1 (22A400)
Report Version: 12
Bridge OS Version: 7.0 (20P420)
Anonymous UUID: F885FB99-C439-51DC-FB8A-19B44CFBD64C
Sleep/Wake UUID: C17EA655-41B9-4F6C-9120-60DD4299EA39
Time Awake Since Boot: 37000 seconds
Time Since Wake: 6199 seconds
System Integrity Protection: enabled
Crashed Thread: 0 Dispatch queue: com.apple.main-thread
Exception Type: EXC_BAD_ACCESS (SIGABRT)
Exception Codes: UNKNOWN_0xD at 0x0000000000000000
Exception Codes: 0x000000000000000d, 0x0000000000000000
VM Region Info: 0 is not in any region. Bytes before following region: 211800064
REGION TYPE START - END [ VSIZE] PRT/MAX SHRMOD REGION DETAIL
UNUSED SPACE AT START
--->
__TEXT c9fd000-ca01000 [ 16K] r-x/r-x SM=COW .../stm32cubeide
Application Specific Information:
abort() called
Thread 0 Crashed:: Dispatch queue: com.apple.main-thread
0 libsystem_kernel.dylib 0x7ff80ea9530e __pthread_kill + 10
1 libsystem_pthread.dylib 0x7ff80eaccf7b pthread_kill + 263
2 libsystem_c.dylib 0x7ff80ea16ca5 abort + 123
3 libjvm.dylib 0x198c7914 os::abort(bool, void*, void const*) + 22
4 libjvm.dylib 0x19a63fdc VMError::report_and_die(int, char const*, char const*, __va_list_tag*, Thread*, unsigned char*, void*, void*, char const*, int, unsigned long) + 2858
5 libjvm.dylib 0x19a6348d VMError::report_and_die(Thread*, unsigned int, unsigned char*, void*, void*, char const*, ...) + 155
6 libjvm.dylib 0x19a6412d VMError::report_and_die(Thread*, unsigned int, unsigned char*, void*, void*) + 33
7 libjvm.dylib 0x198cb6d3 JVM_handle_bsd_signal + 544
8 libjvm.dylib 0x198c92db signalHandler(int, __siginfo*, void*) + 45
9 libsystem_platform.dylib 0x7ff80eaf7c1d _sigtramp + 29
10 JavaScriptCore 0x7ff829246849 JSC::ExecutableAllocator::allocate(unsigned long, JSC::JITCompilationEffort) + 249
11 JavaScriptCore 0x7ff828a8f027 vmEntryToJavaScript + 216
12 JavaScriptCore 0x7ff829230161 JSC::Interpreter::executeCall(JSC::JSGlobalObject*, JSC::JSObject*, JSC::CallData const&, JSC::JSValue, JSC::ArgList const&) + 545
13 JavaScriptCore 0x7ff8294985cb JSC::profiledCall(JSC::JSGlobalObject*, JSC::ProfilingReason, JSC::JSValue, JSC::CallData const&, JSC::JSValue, JSC::ArgList const&, WTF::NakedPtr<JSC::Exception>&) + 107
14 WebCore 0x7ff82cf0dc0b WebCore::JSExecState::profiledCall(JSC::JSGlobalObject*, JSC::ProfilingReason, JSC::JSValue, JSC::CallData const&, JSC::JSValue, JSC::ArgList const&, WTF::NakedPtr<JSC::Exception>&) + 107
15 WebCore 0x7ff82cf4d0ba WebCore::ScheduledAction::executeFunctionInContext(JSC::JSGlobalObject*, JSC::JSValue, WebCore::ScriptExecutionContext&) + 282
16 WebCore 0x7ff82cf4cdb2 WebCore::ScheduledAction::execute(WebCore::Document&) + 194
17 WebCore 0x7ff82bf0a75e WebCore::DOMTimer::fired() + 1614
18 WebCore 0x7ff82d950f48 WTF::Detail::CallableWrapper<WebCore::ThreadTimers::setSharedTimer(WebCore::SharedTimer*)::$_0, void>::call() + 152
19 WebCore 0x7ff82be3974f WebCore::timerFired(__CFRunLoopTimer*, void*) + 31
20 CoreFoundation 0x7ff80ebc0996 __CFRUNLOOP_IS_CALLING_OUT_TO_A_TIMER_CALLBACK_FUNCTION__ + 20
21 CoreFoundation 0x7ff80ebc04fe __CFRunLoopDoTimer + 820
22 CoreFoundation 0x7ff80ebc0114 __CFRunLoopDoTimers + 285
23 CoreFoundation 0x7ff80eba6a5c __CFRunLoopRun + 2098
24 CoreFoundation 0x7ff80eba5bb0 CFRunLoopRunSpecific + 560
25 Foundation 0x7ff80f9fe49a -[NSRunLoop(NSRunLoop) runMode:beforeDate:] + 216
26 libswt-pi-cocoa-4950r5.jnilib 0x39319b29 Java_org_eclipse_swt_internal_cocoa_OS_objc_1msgSend_1bool__JJJJ + 57
27 ??? 0x2b300c87 ???
28 ??? 0x2b8e5d2c ???
Solved! Go to Solution.
2022-11-22 1:13 AM
I confirm that I could reproduce this crash by keeping the application opened displaying the WelcomePage during several minutes.
If I let STM32CubeIDE running after having closed the WelcomePage then I don't reproduce the crash, at least after 30min...
This would be coherent with the crash dump, claiming for an issue in JavaScriptCore, because the only place where the IDE exercices JavaScript is the WelcomePage.
Can you confirm this behavior on your side too?
In the meantime I log an internal ticket, thanks for the report.
2022-11-22 1:13 AM
I confirm that I could reproduce this crash by keeping the application opened displaying the WelcomePage during several minutes.
If I let STM32CubeIDE running after having closed the WelcomePage then I don't reproduce the crash, at least after 30min...
This would be coherent with the crash dump, claiming for an issue in JavaScriptCore, because the only place where the IDE exercices JavaScript is the WelcomePage.
Can you confirm this behavior on your side too?
In the meantime I log an internal ticket, thanks for the report.
2022-11-22 1:32 AM
Hello ron239955_stm1 ,
Thank you for posting your problem.
Could you please delete log files of your workspace (.metdata/.log and .metdata/.ide.log ) ,then louch CubeIDE tool and keep it until it craches to see what happens in the logs at this moment.
Best regards ,
Rim
2022-11-22 10:44 AM
2022-11-22 10:55 AM
2022-11-22 1:43 PM
I can confirm this - I closed the welcome page, and it's been running for a few hours now.
Thanks for the quick response and the helpful suggestion!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.