2024-06-18 1:05 AM
Hello,
I have a working project based on CMake.
I tried to build it under STM32CubeIDE with no success.
Here is the output when trying to build the project:
**** CMake Configure of configuration config_default for project CMakeProject ****
C:\Work\Projets\CMakeProject\Tools\cmake\bin\cmake.exe -S . -B config_default -GUnix Makefiles
CMake Warning:
Ignoring empty string ("") provided on the command line.
-- The C compiler identification is GNU 13.2.1
-- The CXX compiler identification is GNU 13.2.1
-- Detecting C compiler ABI info
-- Detecting C compiler ABI info - failed
-- Check for working C compiler: C:/Work/Projets/CMakeProject/Tools/arm-gnu-toolchain/bin/arm-none-eabi-gcc.exe
-- Check for working C compiler: C:/Work/Projets/CMakeProject/Tools/arm-gnu-toolchain/bin/arm-none-eabi-gcc.exe - broken
CMake Error at Tools/cmake/share/cmake-3.29/Modules/CMakeTestCCompiler.cmake:67 (message):
The C compiler
"C:/Work/Projets/CMakeProject/Tools/arm-gnu-toolchain/bin/arm-none-eabi-gcc.exe"
is not able to compile a simple test program.
It fails with the following output:
Change Dir: 'C:/Work/Projets/CMakeProject/config_default/CMakeFiles/CMakeScratch/TryCompile-5yb5cv'
Run Build Command(s): C:/Work/Projets/CMakeProject/Tools/cmake/bin/cmake.exe -E env VERBOSE=1 C:/Work/Projets/CMakeProject/Tools/ninja-win/ninja.exe -f Makefile cmTC_e738f/fast
ninja: error: Makefile:5: expected '=', got ':'
default_target: all
^ near here
CMake will not be able to correctly generate this project.
Call Stack (most recent call first):
CMakeLists.txt:20 (project)How to make working CMake project work under CubeIDE?
2024-06-20 7:34 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.