2025-12-03 2:35 AM
Hello,
after upgrading from STM32CubeIDE 1.9.0 to 2.0.0 (Eclipse 2024‑09), we encountered a critical issue with Git integration when using SSH and Azure DevOps.
In version 1.9.0, Git operations (pull/push) worked correctly because the IDE allowed selecting an external SSH client (e.g., OpenSSH or PuTTY/Pageant). Azure DevOps recently deprecated ssh-rsa (SHA‑1) and now requires rsa-sha2-256 or rsa-sha2-512 for host key algorithms.
In STM32CubeIDE 2.0.0:
Unable to negotiate key exchange for server host key algorithms.
Client offered: ssh-rsa, ecdsa-sha2-nistp256, ssh-ed25519
Server requires: rsa-sha2-256, rsa-sha2-512
This means SSH with Azure DevOps is currently broken in CubeIDE 2.0.0. The only workarounds are:
Question:
This is a major blocker for teams using Azure DevOps with SSH. Any guidance or roadmap would be appreciated.
Thank you.
2025-12-04 1:32 AM
Hello @los_trpaslikos
This is not a limitation specific to STM32CubeIDE, but rather a broader limitation of the Eclipse platform and its bundled SSH library, which STM32CubeIDE inherits.
I recommend raising this question or reporting the problem on the Eclipse platform as this could help bring attention to the issue and potentially lead to a resolution or workaround.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-12-04 3:59 AM
Thank you for your reply.
I understand that the limitation originates from the Eclipse platform and its use of Apache MINA SSHD. However, STM32CubeIDE integrates Eclipse and distributes it as part of your product. For end users, this issue is a critical blocker because SSH with Azure DevOps is broken out of the box.
Since STM32CubeIDE bundles a specific Eclipse version and JGit/SSH libraries, the responsibility for ensuring compatibility with modern security requirements (such as RSA-SHA2 support) falls on the integrator. Users cannot easily update these libraries themselves without risking IDE stability.
Would ST consider:
Simply redirecting users to Eclipse does not solve the problem for STM32CubeIDE customers, because they rely on your packaged environment.
Thank you for considering this. This is a major blocker for teams using Azure DevOps with SSH.
2025-12-04 4:45 AM
Hello @los_trpaslikos
The migration to a newer Eclipse version within STM32CubeIDE is planned for next year.
In the meantime , use HTTPS for Git operations with Azure DevOps, if possible.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.