2025-11-26 5:28 PM
Hi all,
I have recently installed CubeIDE V2.0 onto my Windows machine - it seems to be working okay.
I have also installed it onto a Linux machine but the link between CubeIDE and CubeMX is broken (CubeIDE opens it as a text file). I have CubeMX installed V6.15.0 - I can run separately.
Someone said to me that for V2.0 I have to set the .ioc editor link manually - does anyone have the detail on how to do that?
Kind regards
Pedro
Solved! Go to Solution.
2025-11-26 5:50 PM
Eclipse : Run an external software in editor view - Stack Overflow
Or run STM32CubeMX as a standalone application and open it there.
2025-11-26 5:50 PM
Eclipse : Run an external software in editor view - Stack Overflow
Or run STM32CubeMX as a standalone application and open it there.
2025-12-04 2:36 PM
Hi,
Although I set the above as a solution, CubeIDE & CubeMX V2.0 on Linux is really bad!
You can't have IDE and MX open at the same time - they lock each other up.
I started a new project with MX, selecting IDE as the project output. The folder layout is weird - main.c is in 2 different locations, and header directories and files are hidden!
I have forced back to V1.9
Kind regards
Pedro
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.