2024-05-04 2:04 PM - edited 2024-05-04 2:05 PM
I have an STM32G474 project that has been working for some time but the latest update doesn't generate code from the .ioc config GUI.
If I make I make changes in the editor and select generate code, the pop flashes quickly and goes away but no code gets generated. I've tried this on a couple of Windows computers with the same result.
2024-05-05 6:45 AM
I got it to work by starting a new project with the same processor. That gave me an error message that I didn't have the right firmware and needed to login and download. The requirement to be logged in is absolutely infuriating BTW.
After getting logged in and having the firmware download, the code would generate. But with an existing project, there was no error message that something was wrong. It would just pop up a window and close it without reporting any problem.
2024-05-07 7:58 AM
Hello @DamageG and welcome to the community,
Could you please check the connection and login to "myST" account to download the firmware and automatically generate the project
Hope this helps!
Thanks,
Rim
2025-07-27 11:48 PM
This is a issue the code gen is just not done no msg or anything - also a newer CubeIDE.do this - @st at least let the user know that Cube has logged out for what ever... just cost me 20min to get that it has nothing to do with my project more with the customer tracking of ST. Do the tracking but don't f. up my UX for it please.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.