2024-03-11 9:55 AM
Hi,
I'm migrating a headless build script we've used before to 1.14.0 - and it seems to fail with all the targets
2024-03-11T16:43:16.0230489Z /opt/st/stm32cubeide_1.14.0/stm32cubeide -data "/home/vsts/work/1/s/2023firmware/ws/" --launcher.suppressErrors -nosplash -application org.eclipse.cdt.managedbuilder.core.headlessbuild -cleanBuild "ThermaWiFi II/Release" -import "/home/vsts/work/1/s/2023firmware/ws/ThermaWiFi II"
2024-03-11T16:43:16.0231124Z ========================== Starting Command Output ===========================
2024-03-11T16:43:16.0258004Z [command]/usr/bin/bash --noprofile --norc /home/vsts/work/_temp/a30f37f7-18a8-48e9-bee1-ca09bd22ec30.sh
2024-03-11T16:43:20.9985098Z Create.
2024-03-11T16:43:21.0173602Z Opening 'ThermaWiFi II'.
2024-03-11T16:43:24.3834526Z 16:43:24 **** Clean-only build of configuration Release for project ThermaWiFi II ****
2024-03-11T16:43:24.4000946Z make -j2 clean
2024-03-11T16:43:24.4601921Z make: *** No rule to make target 'clean'. Stop.
2024-03-11T16:43:24.4738958Z "make -j2 clean" terminated with exit code 2. Build might be incomplete.
2024-03-11T16:43:24.4739581Z
2024-03-11T16:43:24.4740398Z 16:43:24 Build Failed. 1 errors, 0 warnings. (took 87ms)
2024-03-11T16:43:24.4741708Z
2024-03-11T16:43:24.7200784Z 16:43:24 **** Clean-only build of configuration Release for project ThermaWiFi II ****
2024-03-11T16:43:24.7504946Z make -j2 clean
2024-03-11T16:43:24.8122266Z make: *** No rule to make target 'clean'. Stop.
2024-03-11T16:43:24.8177250Z "make -j2 clean" terminated with exit code 2. Build might be incomplete.
2024-03-11T16:43:24.8177710Z
2024-03-11T16:43:24.8178210Z 16:43:24 Build Failed. 1 errors, 0 warnings. (took 97ms)
2024-03-11T16:43:24.8178298Z
2024-03-11T16:43:27.8926585Z 16:43:27 **** Build of configuration Release for project ThermaWiFi II ****
and then fails further down with a missing header.
I've verified all the includes are workspace-relative and the header needed is in the include directories (and in the git repo this clones from)
Any hints?
Mike
Solved! Go to Solution.
2024-03-11 11:03 AM
... and STM32CubeIDE doesnt like spaces or other "special" characters. :)
rename and try again.
2024-03-11 10:30 AM
Project name contains spaces.
2024-03-11 11:03 AM
... and STM32CubeIDE doesnt like spaces or other "special" characters. :)
rename and try again.
2024-03-12 7:54 AM
I can confirm removing the spaces, plus a couple of include case issues (build was on linux, cube was on pc)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.