2021-04-15 12:51 AM
This is the message I receive when debugging for the STM32 Nucleo L476RG Board:
STMicroelectronics ST-LINK GDB server. Version 5.8.0
Copyright (c) 2020, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Debugger connection lost.
Shutting down...
What are the next steps in the debug process? I have updated the firmware as it asked and am also using the latest software for the IDE (1.6.1).
Firmware:
Version: V2J37M27
Build: Oct 22 2020 11:30:39
Software:
STM32CubeIDE 1.6.1
So I believe I am using the most up to date software. Thanks in advance!
2021-04-21 2:11 AM
Hello there!
This issue seems very similar to another thread that is currently being investigated. I would suggest that you follow that thread and try out the suggestions provided by Mattias to see if you can get some additional information.
You can find that link here.
2021-08-03 11:48 PM
Download STM32CubeProgrammer, select "Erasing & Programming" on the left, then do a "Full chip erase", problem solved for my case.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.