2023-07-07 7:30 AM
Hi,
I can't get a simple ST7789 screen working I have tried using this library:- https://github.com/Floyd-Fish/ST7789-STM32 double checked all the connections (including external 8MHZ crystal) and all seems to be fine, I have tried various different settings with the SPI and DMA none of which work. Just wondered if anyone here has had a working program? I am using a simple Nucleo STM32F303K8 MCU. All I get is blank screen.
Solved! Go to Solution.
2023-07-07 3:15 PM
Hi,
I had a similar problem (unsolved) with this driver on a display 2.0TFTSPI GMT020-02 VER:1.1 240x360px (you see blank screen and I see only garbage).
There are some things to look:
1. The Driver.
1.1. This driver needs to configure the GPIOs that you use for CS, DC and RST pins.
1.2. This driver needs to configure the resolution, orientation, displacement...
1.3. I had a warning in compilation about varible types.
It was about 1 year ago. Perhaps the driver version is actually different
2. The hardware: In some sites people says that the display need to be mounted on a PCB, without wires
And however, the SPI configuration
I expect I helped you. I tested with two blue pills and three displays, and never worked. I didn't found the correct combination
2023-07-07 12:35 PM
Perhaps its the hardware..
Link to a site with the actual screen board you purchased.
Show a wiring diagram of exactly how you've wired that board up.
2023-07-07 3:15 PM
Hi,
I had a similar problem (unsolved) with this driver on a display 2.0TFTSPI GMT020-02 VER:1.1 240x360px (you see blank screen and I see only garbage).
There are some things to look:
1. The Driver.
1.1. This driver needs to configure the GPIOs that you use for CS, DC and RST pins.
1.2. This driver needs to configure the resolution, orientation, displacement...
1.3. I had a warning in compilation about varible types.
It was about 1 year ago. Perhaps the driver version is actually different
2. The hardware: In some sites people says that the display need to be mounted on a PCB, without wires
And however, the SPI configuration
I expect I helped you. I tested with two blue pills and three displays, and never worked. I didn't found the correct combination
2023-09-14 11:21 AM
Hi Xisco,
Thanks buddy I found these small SPI screens are fussy about how you connect the SPI wires and power wires and best like too use PCB tracks where possible, I changed my jumper connections and the ST7789 sprang to life!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.