2025-03-22 5:29 AM
"static uint8_t USBD_CDC_DataOut(USBD_HandleTypeDef *pdev, uint8_t epnum)"
In stm32u575 controller and in this function while I am calling
"uint32_t receivedLength = USBD_LL_GetRxDataSize(pdev, epnum);" it gives me 1 insted of 6 or 5 bytes I am reciving so that I could not get entire data
2025-03-22 7:00 AM
Probably the data is being split up into several packets. What program is sending the data?
2025-03-23 11:19 PM
It is a company software.We have to communicate with that.
void HAL_PCD_IRQHandler(PCD_HandleTypeDef *hpcd)
In this function ep->xfer_count += (RegVal & USB_OTG_GRXSTSP_BCNT) >> 4; the xfer_count becomes 1 instead of 6 bytes or 5 bytes we are receiving. If I forcefully put it into 6 .I will get the first entire string.
2025-03-24 4:31 AM
There is a 1 ms delay add while the data is sending from the host software to controller.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.