2025-03-19 8:35 AM
Hi
I'm using the stm32u073, the i2c4 peripheral registers are not visible in the SFR view when debugging, and the peripheral address is not included in the reference manual table 4.
I checked the .svd for u83, is the same.
Cheers
2025-03-19 10:10 AM - edited 2025-03-21 1:50 AM
Salut @max34000 and welcome to the ST Community.
Thank you for escalating those typos (for the RM and the SVD file). I've escalated for correction on the coming release (under internal ticket number 205854).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-03-24 5:15 AM - edited 2025-03-24 5:16 AM
The I2C4 peripheral is missing from the STM32U073.svd file. Probably missed because it isn't available on the whole stm32u0 line.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.