2019-06-28 6:18 AM
How to enable float (printf) in STM32CUBEIDE 1.0.1 IDE?
The -u printf_float option is selected.
2019-07-01 5:30 AM
If you're wondering HOW then that is explained in this thread.
Or, if you're having problems with the float itself that is explained in this thread.
If it was something else completely then please give some more details of the problem you're facing and I'll hopefully be able to provide a better answer.
2019-07-02 4:56 AM
I had problem with printing floats in printf. The solution was to fix the linker file with wrong stack address and I also had to remove the default included file "sysmem.c" since the function _sbrk always failed and malloc was not working.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.