2024-04-15 7:26 PM
Hi I'm KIM from south Korea.
My MCU is "STM32H735ZGT6".
I want to change the clock of ADC1 within the code.
I set up the clock of ADC1 in CUBEMX Clock Configuration about 80Mhz, but I want the clock of ADC1 about 75Mhz.
How can I change the clock?
Thank you.
Solved! Go to Solution.
2024-04-16 6:59 AM
The maximum permissible frequency fADC does not refer to the resolution, but to the implementation of ADC1 and ADC2. ADC1/2 are therefore limited to max. 50MHz with ADC_CR_BOOST=11, fADC of ADC3 is unaffected by this and can be set up to 75MHz.
This also answers your second question: a clock frequency higher than 50MHz can only be used with the ADC3.
Regards
/Peter
2024-04-16 1:47 AM
Please share your IOC so that we can take a look at it, because the clock of ADC1 may be a maximum of 50MHz depending on the setting.
Regards
/Peter
2024-04-16 6:32 AM
I checked that 16bits ADC is up to 50MHz in the datasheet.
But if I use ADC1 or ADC2 as 12bits ADC, can I use it up to 75MHz?
If I want to use 75MHz, is the only way to use ADC3?
2024-04-16 6:59 AM
The maximum permissible frequency fADC does not refer to the resolution, but to the implementation of ADC1 and ADC2. ADC1/2 are therefore limited to max. 50MHz with ADC_CR_BOOST=11, fADC of ADC3 is unaffected by this and can be set up to 75MHz.
This also answers your second question: a clock frequency higher than 50MHz can only be used with the ADC3.
Regards
/Peter
2024-04-16 4:33 PM
Thank you.
I will refer to your advice.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.