2024-09-09 4:25 AM
Hi everyone,
We are facing issue is " Not able to load/dump code via ST -LINK Programmer " and it's showing as error mentioned below. please help us to resolve this kind of issues or please suggest any idea to implement it as soon possible.
--------------------------------------------Cube IDE console output-------------------------------------------------------------------------
STMicroelectronics ST-LINK GDB server. Version 7.8.0
Copyright (c) 2024, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.17.0
-------------------------------------------------------------------
Log output file: C:\Users\tabrezm\AppData\Local\Temp\STM32CubeProgrammer_a11912.log
ST-LINK SN : 002E000A4D46501220383832
ST-LINK FW : V3J15M7B5S1
Board : STLINK-V3SET
Voltage : 3.25V
Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
2nd connect tentative with frequency (8MHz)
ST-LINK SN : 002E000A4D46501220383832
ST-LINK FW : V3J15M7B5S1
Board : STLINK-V3SET
Voltage : 3.26V
SWD freq : 8000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x450
Revision ID : Rev V
Device name : STM32H7xx
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M7
BL Version : 0x90
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a11912.srec
File : ST-LINK_GDB_server_a11912.srec
Size : 65.18 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sector 0
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:00.200
Verifying ...
Error: Data mismatch found at address 0x08000002 (byte = 0x00 instead of 0x08)
Error: Download verification failed
Encountered Error when opening C:\ST\STM32CubeIDE_1.16.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.1.400.202404281720\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Shutting down...
Exit.
Note: please suggest any idea to implement it as soon possible.
Regards,
Lokesh
2024-09-10 2:23 AM
we are using two 2.2uF capacitors are placed and we are getting VCAP is 1 Volt.
and just we compared our schematic and AN4938 Getting started with STM32H74xI/G and STM32H75xI/G MCU hardware development are looks like same then also we are getting VCAP is 1 Volt.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.