2023-03-15 3:42 PM
I have imported an STM32 project, created and debugged in the past using STM32CubeIDE. When I try to build this project in VSCode I see:
Executing task: Build
build task started....
"C:\Program Files\CMake\bin\cmake.EXE" --build "D:/DataRoot/Projects/IO Technologies/IHP Controller/build/debug/build"
The parameter is incorrect
CMake Error: Generator: execution of make failed. Make command was: &&
build finished with error(s).
No changes were made to the imported project.
Please advise how to proceed.
Sid
Solved! Go to Solution.
2023-03-28 1:21 AM
@CsBe it may be blocked by your network admin, if you are on a laptop please connect to an external network without VPN
2023-03-28 6:28 AM
Tryed with other network.. still the same.
> Bundled version of vcpkg: "2023-03-14-105f7f7e8a5ea10dfac9874ff9d1a6bacba5f454".
> Running vcpkg with arguments ["activate","--project","c:\\UserData\\modules\\firmware\\module-1","--json","C:\\Users\\user\\AppData\\Local\\Temp\\44c05403cd0283ca8dd043378a3e08aa"].
warning: vcpkg-artifacts is experimental and may change at any time.
node:internal/modules/cjs/loader:1078
throw err;
^
Error: Cannot find module 'chalk'
Require stack:
- C:\Users\user\AppData\Local\vcpkg\artifacts-2023-03-14\node_modules\vcpkg-ce\ce\dist\cli\format.js
- C:\Users\user\AppData\Local\vcpkg\artifacts-2023-03-14\node_modules\vcpkg-ce\ce\dist\cli\command-line.js
- C:\Users\user\AppData\Local\vcpkg\artifacts-2023-03-14\node_modules\vcpkg-ce\ce\dist\main.js
at Module._resolveFilename (node:internal/modules/cjs/loader:1075:15)
at Module._load (node:internal/modules/cjs/loader:920:27)
at Module.require (node:internal/modules/cjs/loader:1141:19)
at require (node:internal/modules/cjs/helpers:110:18)
at Object.<anonymous> (C:\Users\user\AppData\Local\vcpkg\artifacts-2023-03-14\node_modules\vcpkg-ce\ce\dist\cli\format.js:6:17)
at Module._compile (node:internal/modules/cjs/loader:1254:14)
at Module._extensions..js (node:internal/modules/cjs/loader:1308:10)
at Module.load (node:internal/modules/cjs/loader:1117:32)
at Module._load (node:internal/modules/cjs/loader:958:12)
at Module.require (node:internal/modules/cjs/loader:1141:19) {
code: 'MODULE_NOT_FOUND',
requireStack: [
'C:\\Users\\user\\AppData\\Local\\vcpkg\\artifacts-2023-03-14\\node_modules\\vcpkg-ce\\ce\\dist\\cli\\format.js',
'C:\\Users\\user\\AppData\\Local\\vcpkg\\artifacts-2023-03-14\\node_modules\\vcpkg-ce\\ce\\dist\\cli\\command-line.js',
'C:\\Users\\user\\AppData\\Local\\vcpkg\\artifacts-2023-03-14\\node_modules\\vcpkg-ce\\ce\\dist\\main.js'
]
}
Node.js v18.15.0
> Failed with exit code "1".
> Failed to activate environment at "c:\path\vcpkg-configuration.json".
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.