2023-03-22 7:29 AM
I've been trying for weeks to find and build a project for B-L475-IOT01A that generates an IoT server on AWS, but I can't find anything for STM32CubeIDE that works properly, since I find a lot of failures when building the project when I try with examples from other environments.
If anyone can provide a project, they will be welcome.
Thank you!
2023-03-28 2:34 AM
Hello @Community member and welcome to the Community :),
Are you using SBSFU?
If yes, have a look at this post here: Issue building SBSFU with latest STM32CubeIDE 1.9.0 : here is the solution.
Also, the X-CUBE-AWS 1.4.1 version (STM32 AWS IoT software expansion for STM32Cube) provides many examples. These example developed with IAR, Keil and system Workbench toolchains.
So, try to inspire from the instructions in the readme file to develop your project.
I hope this helps !
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.