2022-07-08 12:02 PM
Hello All,
I am in the process of designing a circuit with four microcontrollers in Daisy chain. I would like to program and debug them via one JTAG port, hence will be daisy chaining them.
Which one of the programmers can do this?. I have used ST-Link-V2, but this cannot programm multiple chips in a daisy chain.
Solved! Go to Solution.
2022-07-11 12:35 AM
Welcome, @ABhuv.1, to the community!
The ST-LINK/V2 is only a simple debugger for SWD (Serial Wire Debugging), for JTAG debugging you need a JTAG debugger, such as the J-LINK. A similar problem has been discussed in the Segger forum, maybe this will help you?
Regards
/Peter
2022-07-11 12:35 AM
Welcome, @ABhuv.1, to the community!
The ST-LINK/V2 is only a simple debugger for SWD (Serial Wire Debugging), for JTAG debugging you need a JTAG debugger, such as the J-LINK. A similar problem has been discussed in the Segger forum, maybe this will help you?
Regards
/Peter
2022-07-11 2:10 AM
HI,
To be more specific, is there a programmer available from STM which can program JTAG chains?
Is the J-Link programmer compatible with Atollic Studio? I cant find any definitive Info on this. From the earlier thread, its isnot clear what IDE was used.
With Regards,
Adi
2022-07-11 2:55 AM
Hello Adi,
Depends what you mean by "From STM", ST-LINK/V2 which is developed by ST can't do it, just as Peter mentioned. However, both STM32CubeIDE and TrueSTUDIO supports J-LINK.
Keep in mind that TrueSTUDIO is deprecated and I would suggest using STM32CubeIDE.
2022-07-11 3:00 AM
Hi Markus,
Thanks for the confirmation. Ill use the Jlink with STM32CubeIDE
With regards,
Adi
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.