2019-05-16 3:45 AM
I just installed STM32CubeIDE 1.0 version to give it a try. When I tried to enable SWV , i saw it is disabled and can not modifiable. At first, I assumed this is because of some limitation of chip, but with same hardware my other compiler ( Keil ) is perfectly using SWV and showing real time variables without stoping the code execution. Am I doing something wrong? How can I enable SWV?
2019-05-16 3:50 AM
For the CM0 parts you need to use the event recorder (EVT?). Keil's Bob Boys has an app note on the method if you dig a bit.
2019-05-16 4:18 AM
I really didn't understand what you mean? I tried to use STM Studio to see variables real time, it is working. So, obviously this hardware ( ST-LINK and STM32F0 ) capable to send variable values via SWO. So, i just want to do same thing in STM32CubeIDE. Whenever I stop execution, IDE is showing the current values of variables, but while running not showing. This EVT, is another way to do this?
2019-05-16 5:11 AM
SWO is just a secondary output stream, similar to the DCC in older ARM devices, and a bit like a USART.
The debugger can already read/write into memory, although I think doing so distorts the execution speed of the target.
2019-05-16 6:28 AM
You may want to look at Segger's RTT. It uses only the minimal Cortex debugger interface and works on M0/F0.
https://www.segger.com/products/debug-probes/j-link/technology/about-real-time-transfer/
See also:
http://blog.atollic.com/the-ultimate-guide-to-etm-instruction-tracing-cortex-m-debugging
With the latest Keil uVision 5.26 I found that using the EVR without RTOS (HAL drivers only) is encumbered. Posted a workaround in this forum earlier.
Good luck.
-- pa
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.