2025-05-28 8:04 AM
I am trying to import and old sw4stm32 (ac6) project into stm32cubeide 1.18.1 but it does not work.
I have tried Migration guide from System Workbench to STM32CubeIDE, UM2579. I can select the import project -> general -> import ac6 systemworkbench for stm32 project. I select the folder with the code and click finish but nothing happens. I do not get any error of success messages and no project appears.
Most of the tutorials/posts are 3 to 6 years old. Is there a new way to import the projects? Is there a log file so I can troubleshoot this?
2025-05-28 8:11 AM
Welcome to the forum.
Please see How to write your question to maximize your chances to find a solution for best results.
@arminBMRT wrote:Most of the tutorials/posts are 3 to 6 years old. Is there a new way to import the projects?
That's around when SW4STM32 was abandoned in favour of CubeIDE.
I guess the assumption is that anyone who had projects to migrate will have done it by now - hence they haven't been maintained/updated.
Do you still have a working SW4STM32 installation?
2025-05-28 8:25 AM
Can you post the example you're trying to import?
I remember opening the .project file seemed to work.
Creating a new project and copying over code is an alternative.
2025-05-28 12:33 PM
> I select the folder with the code and click finish but nothing happens.
Does this folder contain .project and .cproject files? sometimes these files are in a subfolder of the project files.
2025-06-02 1:04 AM
@Andrew Neil Thanks, yes I have an old laptop with the working installation. Is there any way to export it from there?
@TDK Ok this seems to work somewhat. I do get the files loaded but the build says: "Nothing to build for project" I can unfortunately not share the project.
@Pavel A. Yes those files are in the folder but the import does nothing with those I think.
I will try today to update the references in the in the (partially?) imported project
2025-06-02 2:18 AM
@arminBMRT wrote:I have an old laptop with the working installation. Is there any way to export it from there?
I don't know.
But at least that gives you a working reference as a last resort if you have to re-create the project from scratch in CubeIDE...
2025-06-06 8:17 AM
Thanks.
I did not get the importing to work correctly. So I decided to recreate the project from the source manually.
I have tried switching the project to visual studio code with the plugins (going for a modern IDE). I have got it to compile but unfortunately the ethernet PHY was changed in CubeMX. It now only has 2 drivers loaded, which are not on my board. The option to create a custom PHY was removed, so I would need to implement my own driver. This is possible but out of scope for the current project.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.