2022-05-27 12:22 AM
2022-05-27 1:53 AM
No: to do that you would have to have a complete toolchain (compiler, linker, etc) on the Target to compile, link, load, and run the resulting code.
This is the same question as your other thread:
isn't it?
2022-05-27 1:53 AM
No: to do that you would have to have a complete toolchain (compiler, linker, etc) on the Target to compile, link, load, and run the resulting code.
This is the same question as your other thread:
isn't it?
2022-05-27 1:56 AM
but i still searching. i couldnt do anything yet. im stuck :\
2022-05-27 2:09 AM
then continue in the original thread.
I explained there that you need to have the actual HTML, CSS, JS files themselves on the SD card.
You can mark this thread as answered:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.