2023-09-14 2:22 AM
Hello,
I define following constant string, indicating the program version.
static const char version_s[] __attribute__((used)) = "V.10";
This string isn't used in other part of code, but is only defined with the purpose to put in the binary file, a string easy to find, and to make the CRC over the code, depending from the program version.
However, I see that the version string is not included in the binary file, and consequently CRC doesn't depend on it.
Where is the mistake?
Thank you,
Carlo.
Solved! Go to Solution.
2023-09-14 1:41 PM
As @Tesla DeLorean wrote - linkers do removal of unused code. Attribute(used) affects only the compiler, you need something else for the linker. For the GNU linker use a custom section with KEEP in the linker script. For IAR, use specifier __root.
2023-09-14 6:39 AM
If you use the string to calculate a CRC, it'll be included in the binary. How do you know it's not included? When you calculate the CRC, what data is it using? Perhaps show the relevant code.
2023-09-14 8:05 AM
Hello,
I tried to modify the constant string value, but the CRC didn't changed.
So I tried to search the "V.10" string in the .elf file, using a binary editor, and I wasn't able to find it.
2023-09-14 9:52 AM
It sounds more like a program bug than a compiler/linker issue. If you're using the string in the program, the compiler has to include it. It can't optimize it out since it doesn't know how the CRC functions, and all CRC accesses are volatile.
2023-09-14 10:01 AM
If you don't reference things internally the linker is apt to apply dead code removal to discard things.
Check .MAP files for the symbol, and perhaps refer to it or use the KEEP() directive in the Linker Script
2023-09-14 1:41 PM
As @Tesla DeLorean wrote - linkers do removal of unused code. Attribute(used) affects only the compiler, you need something else for the linker. For the GNU linker use a custom section with KEEP in the linker script. For IAR, use specifier __root.
2023-09-15 1:48 AM - edited 2023-09-15 2:20 AM
Thank you @Tesla DeLorean and @Pavel A.
I modified the linker script, adding the new section .ver, with the KEEP directive
.ver :
{
. = ALIGN(4);
KEEP(*(.ver))
. = ALIGN(4);
} >VER
Then I have allocated my constant version string in the new .ver section:
static const char version_s[VERSION_STRING_LEN] __attribute__((section(".ver"), used)) = "V.1";
And now, when I modifiy the version_s[] value, the CRC changes too.
Moreover, I have seen that it works also without specifing the used attribute:
static const char version_s[VERSION_STRING_LEN] __attribute__((section(".ver"))) = "V.1";
In this last case, however, I have the following warning:
warning: 'version_s' defined but not used [-Wunused-const-variable=]
So I prefer to specify also the used attribute.
Thank you,
Carlo
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.