2025-02-26 9:58 AM
Hello everyone,
I want to store configuration data in a flash section that should be retained after updating the code on the controller / flashing a new program. Is this possible using the CubeIDE? If yes, how is it done. If no, can this be done otherwise? As far as I can tell, when downloading the code onto the microcontroller, the whole flash storage will be erased.
Thanks for your help!
2025-02-26 10:02 AM
CubeIDE will only erase as much flash as it needs for the programming:
So just make sure that your "user data" is outside that range
2025-02-26 10:14 AM
My observation sadly does not match with this description. I'm using a STM32H753 Nucleo board. I modified the linker script as follows:
MEMORY
{
RAM_D1 (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
DTCMRAM (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 1920K
USER_FLASH(rw) : ORIGIN = 0x81E0000, LENGTH = 128K
}So, I reserved Bank 2 Sector 7 as my own flash memory. Furthermore, I declared it as NOLOAD:
.user_flash(NOLOAD) :
{
*(.user_flash*);
} > USER_FLASH
But when trying to debug the program using the CubeIDE, the data from these sections is overwritten with 224 bytes of zeros followed by 228 Bytes of ones. (I might have mixed up the amount of zeros and ones here)
2025-02-26 10:18 AM
> CubeIDE will only erase as much flash as it needs for the programming:
But it erases all sectors occupied by the new program and does not restore previous data after the last byte of the programmed data. If your user data is stored in the last sector of the image after the program, make your own tool for updating.
2025-02-26 10:34 AM
@Pavel A. wrote:
[...] it erases all sectors occupied by the new program [...]
Thanks for your reply. Does the USER_FLASH section count as "occupied by the program"?
2025-02-26 11:56 AM
Everything contained in the resulting program counts as occupied by the program. Check the linker map file if not sure.
2025-02-26 12:30 PM
Perhaps use OBJDUMP to establish WHAT in the .ELF file is being put into a NOBITS section.
You can look at the .MAP too, but I tend to use the .ELF as the arbiter of what exactly the linked object is telling the programmer/loader to do.
2025-02-26 3:21 PM
Using objdump -h yields:
➜ Debug objdump -h FLASH_EraseProgram.elf
FLASH_EraseProgram.elf: file format elf32-little
Sections:
Idx Name Size VMA LMA File off Algn
0 .isr_vector 00000298 08000000 08000000 00001000 2**0
CONTENTS, ALLOC, LOAD, READONLY, DATA
1 .text 000026e4 08000298 08000298 00001298 2**2
CONTENTS, ALLOC, LOAD, READONLY, CODE
2 .rodata 00000018 0800297c 0800297c 0000397c 2**2
CONTENTS, ALLOC, LOAD, READONLY, DATA
3 .ARM.extab 00000000 08002994 08002994 00004040 2**0
CONTENTS
4 .ARM 00000000 08002994 08002994 00004040 2**0
CONTENTS
5 .preinit_array 00000000 08002994 08002994 00004040 2**0
CONTENTS, ALLOC, LOAD, DATA
6 .init_array 00000004 08002994 08002994 00003994 2**2
CONTENTS, ALLOC, LOAD, READONLY, DATA
7 .fini_array 00000004 08002998 08002998 00003998 2**2
CONTENTS, ALLOC, LOAD, READONLY, DATA
8 .data 00000040 20000000 0800299c 00004000 2**3
CONTENTS, ALLOC, LOAD, DATA
9 .bss 00000074 20000040 080029dc 00004040 2**3
ALLOC
10 ._user_heap_stack 00000604 200000b4 080029dc 000040b4 2**0
ALLOC
11 .ARM.attributes 0000002e 00000000 00000000 00004040 2**0
CONTENTS, READONLY
12 .debug_info 00008ada 00000000 00000000 0000406e 2**0
CONTENTS, READONLY, DEBUGGING, OCTETS
13 .debug_abbrev 00001774 00000000 00000000 0000cb48 2**0
CONTENTS, READONLY, DEBUGGING, OCTETS
14 .debug_aranges 000006c8 00000000 00000000 0000e2c0 2**3
CONTENTS, READONLY, DEBUGGING, OCTETS
15 .debug_rnglists 00000504 00000000 00000000 0000e988 2**0
CONTENTS, READONLY, DEBUGGING, OCTETS
16 .debug_macro 00034dc7 00000000 00000000 0000ee8c 2**0
CONTENTS, READONLY, DEBUGGING, OCTETS
17 .debug_line 00009059 00000000 00000000 00043c53 2**0
CONTENTS, READONLY, DEBUGGING, OCTETS
18 .debug_str 00152fe1 00000000 00000000 0004ccac 2**0
CONTENTS, READONLY, DEBUGGING, OCTETS
19 .comment 00000043 00000000 00000000 0019fc8d 2**0
CONTENTS, READONLY
20 .debug_frame 00001a1c 00000000 00000000 0019fcd0 2**2
CONTENTS, READONLY, DEBUGGING, OCTETS
21 .debug_line_str 000000ab 00000000 00000000 001a16ec 2**0
CONTENTS, READONLY, DEBUGGING, OCTETSreadelf -S returns:
➜ Debug readelf -S FLASH_EraseProgram.elf
There are 26 section headers, starting at offset 0x1a43e4:
Section Headers:
[Nr] Name Type Addr Off Size ES Flg Lk Inf Al
[ 0] NULL 00000000 000000 000000 00 0 0 0
[ 1] .isr_vector PROGBITS 08000000 001000 000298 00 A 0 0 1
[ 2] .text PROGBITS 08000298 001298 0026e4 00 AX 0 0 4
[ 3] .rodata PROGBITS 0800297c 00397c 000018 00 A 0 0 4
[ 4] .ARM.extab PROGBITS 08002994 004040 000000 00 W 0 0 1
[ 5] .ARM PROGBITS 08002994 004040 000000 00 W 0 0 1
[ 6] .preinit_array PREINIT_ARRAY 08002994 004040 000000 04 WA 0 0 1
[ 7] .init_array INIT_ARRAY 08002994 003994 000004 04 A 0 0 4
[ 8] .fini_array FINI_ARRAY 08002998 003998 000004 04 A 0 0 4
[ 9] .data PROGBITS 20000000 004000 000040 00 WA 0 0 8
[10] .bss NOBITS 20000040 004040 000074 00 WA 0 0 8
[11] ._user_heap_stack NOBITS 200000b4 0040b4 000604 00 WA 0 0 1
[12] .ARM.attributes ARM_ATTRIBUTES 00000000 004040 00002e 00 0 0 1
[13] .debug_info PROGBITS 00000000 00406e 008ada 00 0 0 1
[14] .debug_abbrev PROGBITS 00000000 00cb48 001774 00 0 0 1
[15] .debug_aranges PROGBITS 00000000 00e2c0 0006c8 00 0 0 8
[16] .debug_rnglists PROGBITS 00000000 00e988 000504 00 0 0 1
[17] .debug_macro PROGBITS 00000000 00ee8c 034dc7 00 0 0 1
[18] .debug_line PROGBITS 00000000 043c53 009059 00 0 0 1
[19] .debug_str PROGBITS 00000000 04ccac 152fe1 01 MS 0 0 1
[20] .comment PROGBITS 00000000 19fc8d 000043 01 MS 0 0 1
[21] .debug_frame PROGBITS 00000000 19fcd0 001a1c 00 0 0 4
[22] .debug_line_str PROGBITS 00000000 1a16ec 0000ab 01 MS 0 0 1
[23] .symtab SYMTAB 00000000 1a1798 0019c0 10 24 198 4
[24] .strtab STRTAB 00000000 1a3158 00116e 00 0 0 1
[25] .shstrtab STRTAB 00000000 1a42c6 00011c 00 0 0 1I can't find any part of the USER_FLASH memory range in any of those outputs.
2025-02-27 3:35 PM
> I can't find any part of the USER_FLASH memory range in any of those outputs.
Then by default (normally) both CubeIDE loader/debugger and CubeProgrammer won't touch the USER_FLASH sector. Check the options for flashing.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.