2024-04-12 10:27 PM - edited 2024-04-13 12:13 AM
I want to interface STM32H750xB with ST-Link/V2 debugger using TAG connector
TAG-Connect™ Pin-Out
The Tag-connect provides SWD, USART and USB interfaces for debug, control, and
monitoring the MCU. Table 1 provides TAG-connect connector DBG1 pin-out details.
Pin Signal Name Description
1 VCC3 +3.3V SOM power supply
2 NRST System reset
3 SWCLK/JTCK Serial wire clock/JTAG test clock
4 SWDIO/JTMS Serial wire data in/out//JTAG test mode select
5 USART1_TX USART1 Transmit data
6 USART1_RX USART1 Receive data
7 USB_FS1_VBUS USB FS OTG port 1 VBUS input
8 USB_FS1_DM USB FS OTG port 1 data - line
9 USB_FS1_DP USB FS OTG port 1 data + line
10 GND SOM ground
2024-04-12 11:40 PM
You write > How to i interface STM32H750xB with ST-Link/V2 <
and then show the interface you want to use (or build a new board ?) - fine.
And whats the problem then ?
2024-04-12 11:41 PM
In normal situation required is pins 10,3,4
good is add too 2.
2024-04-13 12:08 AM
But as per what i know pin 3 (JTCK) is for clock And pin 4 (JTMS) for mode selection so we need other pins to transmit and receive data i.e USART1 Tx and Rx
I have only worked on boards which have inbuilt stlink so it would automatically generate code in cube ide
so i have no idea how to write a code for it so any references would be helpful
Thank You
2024-04-13 12:22 AM
Used signals is SWCLK SWDIO and i dont understand your Q about code. Working with code is exatly same.
Connect STLinkv2 USB to PC run IDE and use it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.