2021-02-15 10:38 AM
When I try to open debug configurations for a makefile based project, CubeIDE throws an error popup - Java null something.
So I cannot create new debug config for the project.
Workaround: created a small dummy project for the same target, created a debug config for it,
then added the binary from the makefile project to load.
Edited it, selected not to build, only load with symbols. And the "donor" project binary - not anything.
This way I've managed to debug it.
By the way, cannot make ITM_send_char working in CubeIDE. In Atollic it (mostly) works.
Indeed there's some bug...
/* After a long affair with Atollic I'm forced to use CubeIDE because customer wants it.
Unfortunately it still feels very beta vs. the Atollic */
2021-02-15 12:11 PM
Hi Pavel,
> cannot make ITM_send_char working
ITM_SendChar
What MCU? Even if you set the correct core + SWD clock in the debug tab? Works here.
KnarfB
2021-02-15 12:40 PM
STM32H743 at 400 MHz
2021-02-15 1:02 PM
Hmm. I don't have a H7 board. F4 F7 L4 G4 do work, if one follows AN4989 "STM32 microcontroller debug toolbox", strange.
2021-02-16 4:15 AM
possibly related:
2021-02-18 12:44 PM
Update on the ITM prints:
I'm doing the following for the test:
ITM_SendChar('\n');
ITM_SendChar('a');
ITM_SendChar('\n');Of course enabled the ITM output at the main() breakpoint.
After running thru these 3 lines nothing appears in the ITM data console.
Then I close "Port 0" tab, click on configure, enable Port 0 again and close configure dialog.
Then Port 0 tab opens again and... my character "a" is right there. So it has been received, it's the IDE not wanting to show it for unknown reason.
Weird!
-- pa
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.