2023-08-21 9:39 PM
Hi everyone,
i am working on a STM32C011F6P6
i am trying to apply some I2C setting to other chip
normal writing value to corresponding address
but seems the HAL_I2C_Mem_Write function is stucked
these are the read and write function
HAL_StatusTypeDef i2c_write_reg(uint8_t reg, uint8_t send_data ) {
return HAL_I2C_Mem_Write(&hi2c1, SLAVE_ADDRESS<<1 , reg, I2C_MEMADD_SIZE_8BIT ,&send_data, 1 , HAL_MAX_DELAY);
}
uint8_t i2c_read_reg(uint8_t reg) {
uint8_t temp;
if (HAL_I2C_Mem_Read(&hi2c1, SLAVE_ADDRESS << 1, reg, I2C_MEMADD_SIZE_8BIT, &temp, 1, HAL_MAX_DELAY) != HAL_OK) {
// Handle error here
return 0; // Or any default value you prefer
}
return temp; // Success, return the read value
}
these are the code execute
HAL_StatusTypeDef stat2;
stat2 = i2c_write_reg(0x25,0x70);
if(stat2!=HAL_OK){
printf("HAL not ok\r\n");
}
stat2 =i2c_write_reg(0x26,0x07);
if(stat2!=HAL_OK){
printf("HAL not ok\r\n");
}
uint8_t x ;
x = i2c_read_reg(0x25) ;
printf("0x250x%02x\r\n",x);
x = i2c_read_reg(0x26) ;
printf("0x26:0x%02x\r\n",x);
i already have pull up resistor on board
any solution or any thing i can do to identify the real issue?
2023-08-22 12:50 AM
any solution or any thing i can do to identify the real issue?
I don't know if it can help in your case, but I found these videos about advanced debugging:
STM32CubeIDE Advanced Debug Features
https://youtube.com/playlist?list=PLnMKNibPkDnEDEsV7IBXNvg7oNn3MfRd6
2023-08-22 6:48 AM - edited 2023-08-22 6:48 AM
Always use HAL_I2C_IsDeviceReady first to verify the device is responding before using other functions.
My guess is the bus is stuck to due debugging/previous activity on bus. In which case you need to toggle SCL 9 times at startup before initializing it as I2C. Or power cycle everything.
If HAL_I2C_IsDeviceReady does not pass for this chip, then problem could be somewhere else.
2023-08-22 8:31 PM
just found is my slave device have not powered at the first place
now it can return hal_err
thinking why it is not working
2023-08-23 3:28 AM
Hello @uveuvenouve ,
I suggest you use an oscilloscope to check SDA and SCL behavior or try to debug and set breakpoints .
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-08-23 6:37 AM
If your slave device is not powered, it's not likely to respond to commands. It will also generally pull the SDA and SCL lines down and prevent you from using them effectively.
2023-08-23 7:39 PM
just found i may have messed up the slave id setting
i thought setting slave id in i2c mean the target slave device
but seems that is stating own slave id
and i have 2 devices connected to the target slave device
so i think they some how conflicted by falsely setting all 3 devices have same slave id
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.