2024-08-27 10:20 PM
we are facing following errors during compilation:
1. fatal error: cmsis_os2.h: No such file or directory OSWrappers.cpp /STM32U5G9J-DK2/Application/User/TouchGFX/target/generated line 22 C/C++ Problem
2.Description Resource Path Location Type
fatal error: cmsis_os2.h: No such file or directory STM32U5G9J-DK2 line 24 C/C++ Problem
3.Description Resource Path Location Type
fatal error: nema_sys_defs.h: No such file or directory nema_hal.c /STM32U5G9J-DK2/Application/User/TouchGFX/target/generated line 31 C/C++ Problem
4.Description Resource Path Location Type
fatal error: touchgfx_nema/HALGPU2D.hpp: No such file or directory STM32U5G9J-DK2 line 21 C/C++ Problem
5.Description Resource Path Location Type
fatal error: touchgfx_nema/LCDGPU2D.hpp: No such file or directory TouchGFXConfiguration.cpp /STM32U5G9J-DK2/Application/User/TouchGFX/target/generated line 24 C/C++ Problem
2024-08-28 1:35 AM - edited 2024-08-28 1:36 AM
Hello @aiswarya ,
It seems that you have missing or incorrect paths.
So, ensure that all required include paths are correctly set up in your project settings.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.