2025-07-19 11:31 PM - edited 2025-07-21 11:45 PM
Dear @Tesla DeLorean and @KDJEM.1
I am using NUCLEO-G491RE board and i want to create external flash loader for W25Q64JVSSIQ QSPI flash memory. I used external loader files from Github and build the .stldr file and placed in CubeProgrammer. when i try to read from 0x90000000 location, i am getting read failure error. I used the below path to create external loader for W25Q64JVSSIQ QSPI flash memory,
Driver code is working fine since I am able to see the data in memory mapped mode with test code provided in the github link.
But, when create a external loader using github files and placed .stldr file into cubeprogrammer and working on read/write/erase and these operations are failing.
Could you please check my project and do needful. PFA for my loader project
Thanks
2025-07-28 4:48 PM
Hi @Tesla DeLorean ,
G474 and G491 are same in implementation as per my knowledge
2025-08-03 9:09 PM
Hi @KDJEM.1
Did you check the code that is attached to above. If not yet could you please check and let me know where is actual issue.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.