2024-04-30 1:01 AM
Assistance Needed: Ethernet Configuration Issue on STM32F429IIT6
I'm encountering difficulties in enabling Ethernet functionality on the STM32F429IIT6 board. Despite efforts, I can't ping the Ethernet connection. Could you provide example code or guidelines for configuring Ethernet? I'll also attach the pin connection and schematic for review. Your prompt assistance would be greatly appreciated.
this is my main code
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_LWIP_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
MX_LWIP_Process();
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
Thank you,
Akshay.
2024-04-30 1:11 AM
Could you provide example code or guidelines for configuring Ethernet? I'll also attach the pin connection and schematic for review. Your prompt assistance would be greatly appreciated.
LWIP examples here: https://github.com/STMicroelectronics/STM32CubeF4/tree/master/Projects/STM324x9I_EVAL/Applications/LwIP
Schematics of the board (STM32F429-EVAL) using ETH MII mode: https://www.st.com/resource/en/schematic_pack/mb1045-f429nih6-b08_schematic.pdf
2024-05-01 3:03 AM
I'm currently working with an RMII configuration and trying to integrate FreeRTOS into my system, but I'm still unable to establish a ping connection with the board.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.