2024-05-01 5:36 AM - edited 2024-05-01 6:38 AM
Searching for "USBX" in the forum brings up over 330 post. USBX is deprecated since 2014, but a requirement for it still lingers in st-stlink-server-2.1.1-1-linux-amd64.rpm
# unzip en.st-stm32cubeide_1.15.1_21094_20240412_1041_amd64.rpm_bundle.sh.zip
# sh en.st-stm32cubeide_1.15.1_21094_20240412_1041_amd64.rpm_bundle.sh
...
License accepted.
Do you want to install Segger J-Link udev rules? [Y/n] n
error: Failed dependencies:
libusbx >= 1.0 is needed by st-stlink-server-2.1.1-1.x86_64
Preparing... ################################# [100%]
To work around:
- install rpmrebuild
- run "sh st-stm32cubeide_1.15.1_21094_20240412_1041_amd64.rpm_bundle.sh" again, but do not type anything in the license window
- Put the installer in the background with "^z^ or open another terminal where the unzip happened
#cd makeself_dir_AvZtzf/
#rpmrebuild -e -p st-stlink-server-2.1.1-1-linux-amd64.rpm
Remove the line "Requires: libusbx >= 1.0" in the editor that opened up
Save and exit
...
result: /usr/src/packages/RPMS/x86_64/st-stlink-server-2.1.1-1.x86_64.rpm
- install /usr/src/packages/RPMS/x86_64/st-stlink-server-2.1.1-1.x86_64.rpm
- install st-stm32cubeide-1.15.1-21094_20240412_1041.amd64.rpm
- if needed also install st-stlink-udev-rules-1.0.3-2-linux-noarch.rpm
- Go back to the installer window and type no to clean up
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.