2024-05-07 7:35 AM
Hello all,
I am currently working on a project that involves utilizing the Ethernet peripheral on the Nucleo-H743ZI2 development board. While researching implementation options, I noticed that many resources recommend using the LwIP stack for handling Ethernet communication. However, for various reasons specific to my project requirements, I would prefer to avoid using the LwIP stack.
Could you please provide any resources, code examples on how to utilize the Ethernet peripheral with STM32Cube_FW_H7_V1.11.2 on the Nucleo-H743ZI2 board without relying on the LwIP stack? I am particularly interested in:
2024-05-07 8:30 AM
FreeRTOS, ThreadX/NetX and other RTOS work on STM32 and have their own network stack. Consider using these.
Or roll your own network drivers even not based on TCP/IP.
However, there are no ready examples for the latter, you can use available LwIP examples or find a consultant.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.