2024-05-06 3:49 PM - edited 2024-05-06 3:51 PM
Hi,
I want to enable the global interrupt for TIM3 so that I can recognize when it becimes active (it raises the pin).
I've added:
if(htim_base->Instance==TIM3)
{
/* Peripheral clock enable */
__HAL_RCC_TIM3_CLK_ENABLE();
/* TIM2 interrupt Init */
HAL_NVIC_SetPriority(TIM3_IRQn, 5, 0);
HAL_NVIC_EnableIRQ(TIM3_IRQn);
}
this to my void HAL_TIM_Base_MspInit(TIM_HandleTypeDef* htim_base) and can confirm that it gets executed and finally added
void TIM3_IRQHandler(void)
{
HAL_TIM_IRQHandler(&htim3);
}
into stm32f4xx_it.c but I still don't get a TIM3 callback in void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim). What am I missing?
I can see the PWM waveform on my scope but TIM3_IRQHandler() never gets invoked
Solved! Go to Solution.
2024-05-07 2:49 AM - edited 2024-05-07 2:49 AM
Hello @debug,
Try to enable the update interrupt (UIE) for TIM3, you can enable it by setting the DIER register or by HAL using __HAL_TIM_ENABLE_IT(&htim3, TIM_IT_UPDATE);
Also, are you starting the timer with HAL_TIM_Base_Start_IT(&htim3) or HAL_TIM_Base_Start(&htim3)?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-07 2:49 AM - edited 2024-05-07 2:49 AM
Hello @debug,
Try to enable the update interrupt (UIE) for TIM3, you can enable it by setting the DIER register or by HAL using __HAL_TIM_ENABLE_IT(&htim3, TIM_IT_UPDATE);
Also, are you starting the timer with HAL_TIM_Base_Start_IT(&htim3) or HAL_TIM_Base_Start(&htim3)?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-07 8:27 AM
Yes, calling __HAL_TIM_ENABLE_IT(&htim3, TIM_IT_UPDATE); did the trick! Thanks!
I actually have built a custom start function "HAL_TIM_PWM_Start_custom()" to be able to setup timers completely and then just need to call __HAL_TIM_ENABLE(&htim3); to start them (because I want to start two back-to-back with minimal latency).
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.