2025-07-10 6:32 AM
Hello,
Previously I had CubeMX 6.13.0 and here is the code which was autogenerated and working as expected for RS485 communication, where I have manually handled the Direction pin in my code.
static void MX_LPUART1_UART_Init(void)
{
hlpuart1.Instance = LPUART1;
hlpuart1.Init.BaudRate = 115200;
hlpuart1.Init.WordLength = UART_WORDLENGTH_8B;
hlpuart1.Init.StopBits = UART_STOPBITS_1;
hlpuart1.Init.Parity = UART_PARITY_NONE;
hlpuart1.Init.Mode = UART_MODE_TX_RX;
hlpuart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
hlpuart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
hlpuart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_RS485Ex_Init(&hlpuart1, UART_DE_POLARITY_HIGH, 0, 0) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetTxFifoThreshold(&hlpuart1, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetRxFifoThreshold(&hlpuart1, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_DisableFifoMode(&hlpuart1) != HAL_OK)
{
Error_Handler();
}
}
Now I have updated the CubeMX version to 6.15.0 and latest stm32cube , which fails the RS485 communication:
static void MX_LPUART1_UART_Init(void)
{
hlpuart1.Instance = LPUART1;
hlpuart1.Init.BaudRate = 115200;
hlpuart1.Init.WordLength = UART_WORDLENGTH_8B;
hlpuart1.Init.StopBits = UART_STOPBITS_1;
hlpuart1.Init.Parity = UART_PARITY_NONE;
hlpuart1.Init.Mode = UART_MODE_TX_RX;
hlpuart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
hlpuart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
hlpuart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
hlpuart1.FifoMode = UART_FIFOMODE_ENABLE;
if (HAL_UART_Init(&hlpuart1) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetTxFifoThreshold(&hlpuart1, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetRxFifoThreshold(&hlpuart1, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_EnableFifoMode(&hlpuart1) != HAL_OK)
{
Error_Handler();
}
if (HAL_RS485Ex_Init(&hlpuart1, UART_DE_POLARITY_HIGH, 0, 0) != HAL_OK)
{
Error_Handler();
}
}
Then I did these changes (re-arrange HAL_RS485Ex_Init() function position), and it works, but as this code is autogenerated multiple times which increase my re-work to arrange the code again and again.
static void MX_LPUART1_UART_Init(void)
{
hlpuart1.Instance = LPUART1;
hlpuart1.Init.BaudRate = 115200;
hlpuart1.Init.WordLength = UART_WORDLENGTH_8B;
hlpuart1.Init.StopBits = UART_STOPBITS_1;
hlpuart1.Init.Parity = UART_PARITY_NONE;
hlpuart1.Init.Mode = UART_MODE_TX_RX;
hlpuart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
hlpuart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
hlpuart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
hlpuart1.FifoMode = UART_FIFOMODE_ENABLE;
if (HAL_UART_Init(&hlpuart1) != HAL_OK)
{
Error_Handler();
}
if (HAL_RS485Ex_Init(&hlpuart1, UART_DE_POLARITY_HIGH, 0, 0) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetTxFifoThreshold(&hlpuart1, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetRxFifoThreshold(&hlpuart1, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_EnableFifoMode(&hlpuart1) != HAL_OK)
{
Error_Handler();
}
}As if we initialize uart or rs485 before fifo threshold setting or fifo enable then code works or else it receives the data but not transmit it or give response on TX.
Also using low level driver library in another project instead of HAL so there also the same issue. I have attached an ioc file of that project as well:
void MX_LPUART1_UART_Init(void)
{
/* USER CODE BEGIN LPUART1_Init 0 */
/* USER CODE END LPUART1_Init 0 */
LL_LPUART_InitTypeDef LPUART_InitStruct = {0};
LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
LL_RCC_SetLPUARTClockSource(LL_RCC_LPUART1_CLKSOURCE_PCLK1);
/* Peripheral clock enable */
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_LPUART1);
LL_IOP_GRP1_EnableClock(LL_IOP_GRP1_PERIPH_GPIOB);
/**LPUART1 GPIO Configuration
PB10 ------> LPUART1_RX
PB11 ------> LPUART1_TX
PB12 ------> LPUART1_DE
*/
GPIO_InitStruct.Pin = LL_GPIO_PIN_10|LL_GPIO_PIN_11;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_UP;
GPIO_InitStruct.Alternate = LL_GPIO_AF_8;
LL_GPIO_Init(GPIOB, &GPIO_InitStruct);
GPIO_InitStruct.Pin = LL_GPIO_PIN_12;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_DOWN;
GPIO_InitStruct.Alternate = LL_GPIO_AF_8;
LL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* LPUART1 interrupt Init */
NVIC_SetPriority(USART3_LPUART1_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),0, 0));
NVIC_EnableIRQ(USART3_LPUART1_IRQn);
/* USER CODE BEGIN LPUART1_Init 1 */
/* USER CODE END LPUART1_Init 1 */
LPUART_InitStruct.PrescalerValue = LL_LPUART_PRESCALER_DIV1;
LPUART_InitStruct.BaudRate = 115200;
LPUART_InitStruct.DataWidth = LL_LPUART_DATAWIDTH_8B;
LPUART_InitStruct.StopBits = LL_LPUART_STOPBITS_1;
LPUART_InitStruct.Parity = LL_LPUART_PARITY_NONE;
LPUART_InitStruct.TransferDirection = LL_LPUART_DIRECTION_TX_RX;
LPUART_InitStruct.HardwareFlowControl = LL_LPUART_HWCONTROL_NONE;
LL_LPUART_Init(LPUART1, &LPUART_InitStruct);
LL_LPUART_SetTXFIFOThreshold(LPUART1, LL_LPUART_FIFOTHRESHOLD_1_8);
LL_LPUART_SetRXFIFOThreshold(LPUART1, LL_LPUART_FIFOTHRESHOLD_1_8);
LL_LPUART_EnableFIFO(LPUART1);
/* USER CODE BEGIN WKUPType LPUART1 */
/* USER CODE END WKUPType LPUART1 */
LL_LPUART_Enable(LPUART1);
LL_LPUART_Init(LPUART1, &LPUART_InitStruct);
LL_LPUART_SetTXFIFOThreshold(LPUART1, LL_LPUART_FIFOTHRESHOLD_1_8);
LL_LPUART_SetRXFIFOThreshold(LPUART1, LL_LPUART_FIFOTHRESHOLD_1_8);
LL_LPUART_EnableDEMode(LPUART1);
LL_LPUART_SetDESignalPolarity(LPUART1, LL_LPUART_DE_POLARITY_LOW);
LL_LPUART_SetDEAssertionTime(LPUART1, 0);
LL_LPUART_SetDEDeassertionTime(LPUART1, 0);
LL_LPUART_EnableFIFO(LPUART1);
LL_LPUART_Enable(LPUART1);
/* USER CODE BEGIN LPUART1_Init 2 */
/* USER CODE END LPUART1_Init 2 */
}
Surprising by latest cubemx version why function calling sequence updated and code suddenly stopped working after upgrade.
Please any expert or ST Employee can help us...
Thanks & Regards,
Mahendra Rana
2025-07-10 9:33 AM
Hello @MAHENDRA_RANA
Thank you for binging this issue to our attention,
I will check it internally and get back to you asap.
KR,
Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-07-11 12:42 AM
2025-07-16 12:53 AM
Is there any update for solution of issue created by latest cubemx?
Regards,
Mahendra Rana
2025-07-18 9:06 AM
Hello @MAHENDRA_RANA
This issue has been escalated to the relevant team for fixing (Internal ticket number: 214438: Internal ticket number is only for reference, not accessible or usable outside of ST).
KR,
Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-08-20 3:09 AM
Can you please update on our issue. How to fix it or any update on your internal ticket no. 214438.
Regards,
Mahendra Rana
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.