2025-05-11 3:48 AM
Hello!
When I build my project, I get these errors. I should note that the header files are in the driver folder, and I have added all the necessary include paths.
"C:/Users/helat/STM32CubeIDE/workspace_1.18.1/PFA-SecureM/Core/Src/main.c:90:(.text.main+0xc): undefined reference to `MX_GPIO_Init'
C:/ST/STM32CubeIDE_1.18.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/Users/helat/STM32CubeIDE/workspace_1.18.1/PFA-SecureM/Core/Src/main.c:91:(.text.main+0x10): undefined reference to `MX_ICACHE_Init'
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:70: PFA-SecureM.elf] Error 1
"make -j20 all" terminated with exit code 2. Build might be incomplete."
Solved! Go to Solution.
2025-05-11 7:13 AM
> undefined reference to `MX_ICACHE_Init'
This means that MX_ICACHE_Init has been used prior to its definition. Ensure it is being defined before used.
If this code is directly generated from an IOC, please include that IOC. Otherwise please include your project code files.
2025-05-11 3:56 AM - edited 2025-05-11 8:21 AM
those are linker errors. check the source folders/files that will be linked. C++ issues?
> When I build my project,
Nobody here knows your project.
How to write your question to maximize your chance... - STMicroelectronics Community
hth
KnarfB
2025-05-11 7:13 AM
> undefined reference to `MX_ICACHE_Init'
This means that MX_ICACHE_Init has been used prior to its definition. Ensure it is being defined before used.
If this code is directly generated from an IOC, please include that IOC. Otherwise please include your project code files.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.