2025-08-08 12:34 AM
Hello,
I have an issue with this setup:
Nothing is implemented regarding the SPI port yet.
I succesfully went through this STM tutorial: https://www.youtube.com/watch?v=LdY2bieaPwk
Success means: when I switch the PC13 button, the string "Hello World" is transmitted to the terminal on my PC.
Here is the But:
A thread for the blinking of an LED is not running anymore:
VOID LD1_thread_entry(ULONG initial_input){
(VOID)initial_input;
while(1){
HAL_GPIO_TogglePin(LED_RD1_o_GPIO_Port,LED_RD1_o_Pin);
tx_thread_sleep(8); // 1tick per 10ms
}
}I know the workaround already:
But my understanding is lacking here:
The usbx process is just this:
VOID usbx_cdc_acm_write_thread_entry(ULONG thread_input)
{
UX_PARAMETER_NOT_USED(thread_input);
ULONG actual_length;
while(1)
{
// wait for button press
tx_semaphore_get(&semaphore, TX_WAIT_FOREVER);
// transmit data
ux_device_class_cdc_acm_write(cdc_acm, (UCHAR *)(&Tx_Buffer), (strlen(Tx_Buffer)), &actual_length);
}
}So all the time while I am not pressing the button, usbx_write_thread is just waiting for the semaphore. By definition is "sleeping" until semaphore wakes the thread up.
But how can this sleeping-process prevent a (low priority) task (LED blinking) from being executed?
The concept of ThreadX is that exactly this should never happen.
I would be grateful if someone knows where "the bug" is.
In case you need more information about the background/code/... just let me know. Right now my code really looks like in the tutorial plus the LED stuff.
Thanks in advance!
Enrico
Solved! Go to Solution.
2025-08-12 7:12 AM
Bug was fixed:
the issue was a while(1) loop. In the tutorial this while(1); was suggested in the function app_ux_device_thread_entry() in app_usbx_device.c by the tutorial. But it blocks the other (low priority) tasks from being executed.
This function is just for configuration so, the while(1) can simply be deleted.
2025-08-12 7:12 AM
Bug was fixed:
the issue was a while(1) loop. In the tutorial this while(1); was suggested in the function app_ux_device_thread_entry() in app_usbx_device.c by the tutorial. But it blocks the other (low priority) tasks from being executed.
This function is just for configuration so, the while(1) can simply be deleted.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.