2022-12-27 12:00 AM - last edited on 2025-03-27 6:53 AM by Andrew Neil
Good afternoon dear collegues!
When I try to compile and upload my program through the CubeIDE I have the following problem:
Error: Data mismatch found at address 0x080003C0 (byte = 0x1B instead of 0x1A)
Error: Download verification failed
Every time the byte is different. I use Stm32F072CBT6 MCU and Stm32F030C8T6.
I try to programm it with StLink board
Now on my board the Boot Pin (Boot -- 10k -- GND) and NRST pin (NRST -- C -- GND) are connected only.
Is this problem connected with CubeIDE?
2022-12-27 4:28 AM
More apt to be a device or power supply issue
2022-12-30 4:40 AM
Hello @MMudr.1
First let me thank you for posting.
Did you checked the hw like @Community member mentioned?
I want to suggest if you try to flash the MCU with CubePorgrammer.
Kind regards,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.