cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX generated code error when using BSP code

Giovanni1
Associate

Hello all.

I'm new here, this is my first post.

I found a problem with STM32CubeIDE.

I don't know where to post errors report, so please move this post if this is the wrong place.

I'm a skilled embedded programmer, but I've worked till now on 8 bit microcontroller (AVR, PIC, STM8, Z80, etc.).

Now we (me and my company) are moving to the ARM platform, and I choose STM32 as our next family of MCU/MPU.

We need two different platform, for different devices: an high performance one, for which I choose the Cortex-M33 (STM32H5 family) and a low power, low cost one, for which I choose instead the STM32C0+ (STM32C071).

I bought few NUCLEO boards, so I can learn the new ecosystem in an easy way.

I installed STM32CubeIDE, complete with CubeMX.

I created a new STM32 project, using the board selector I choose the NUCLEO-H563ZI board.

Using CubeMX I configured the board; I also enabled BSP HMI code generation, and enabled User Leds.

I decided to use ThreadX and NetXDuo.

Now, there's a little problem: When I create the CubeMX code, there's an error in the main() function generated by CubeMX.

The CubeMX code generator insert the instruction "MX_ThreadX_Init()" before the BSP initialization code, just below the "USER CODE END 2" comment; so, User Leds and virtual coms do not work, since their initialization code is never executed (once you call  MX_ThreadX_Init() it never returns);

I have to manually move it from there to just before the "while (1)" statement at the end of main().

This is not a big problem, but is an annoying one; for a beginner it can frustrating.

Here below an extract of the main() code generated by CubeMX:

 

 

  /* USER CODE BEGIN SysInit */

  /* USER CODE END SysInit */

  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_ETH_Init();
  MX_ICACHE_Init();
  /* USER CODE BEGIN 2 */

  /* USER CODE END 2 */

  MX_ThreadX_Init();

  /* Initialize leds */
  BSP_LED_Init(LED_GREEN);
  BSP_LED_Init(LED_YELLOW);
  BSP_LED_Init(LED_RED);

  /* Initialize USER push-button, will be used to trigger an interrupt each time it's pressed.*/
  BSP_PB_Init(BUTTON_USER, BUTTON_MODE_EXTI);

  /* Initialize COM1 port (115200, 8 bits (7-bit data + 1 stop bit), no parity */
  BspCOMInit.BaudRate   = 115200;
  BspCOMInit.WordLength = COM_WORDLENGTH_8B;
  BspCOMInit.StopBits   = COM_STOPBITS_1;
  BspCOMInit.Parity     = COM_PARITY_NONE;
  BspCOMInit.HwFlowCtl  = COM_HWCONTROL_NONE;
  if (BSP_COM_Init(COM1, &BspCOMInit) != BSP_ERROR_NONE)
  {
    Error_Handler();
  }

  /* We should never get here as control is now taken by the scheduler */

  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {

    /* USER CODE END WHILE */

    /* USER CODE BEGIN 3 */
  }
  /* USER CODE END 3 */

 

 

You can see, at line 14, the MX_ThreadX_Init() instruction, that should instead  be located under line 34.

2 REPLIES 2
Mahmoud Ben Romdhane
ST Employee

Hello @Giovanni11,

First let me thank you for posting and welcome to the ST Community.

Your request is under investigation, and I will get back to you ASAP.

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Andrew Neil
Super User

As a workaround, you can set CubeMX to not generate the calls to the init functions - so then you can insert them in the order you choose:

https://community.st.com/t5/stm32cubemx-mcus/how-to-have-cubemx-configure-a-peripheral-but-not-enable-it/m-p/761680/highlight/true#M30800

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.