2024-01-20 12:43 AM - edited 2024-01-20 12:44 AM
Hello everyone, can someone tell me why casting doesn't work. I want to convert int values of an array to float.
for (int i = 0; i<= adcBufferSize; i++)
{
adc_buffer_float[i] = (float)adc_buffer [i];
}
2024-03-24 5:24 AM
I have the same problem. I read analog values with my ADC and values are type of uint16_t but when i convert my array of values that i get from ADC (Because of doublebuffering) to Float numbers get weird. Is it because of endians, maby overflows i dont know. I have it all on my work PC but i can get a screenshot tomorow.
I have tried
for(int n = 0;n < BuffSize;n++){
FLOATARRAY[n] = (float) INTARRAY[n] * 1.0f;
}
2024-03-24 9:31 AM
You'll need to show the definitions, and datasets which are failing, to have any idea as to why the presented code fragment is failing.
I doubt it's got anything to do with endian ordering or overflow, as a float should have no trouble representing a number in the 0-65535 range. Where you'll get issues is 8 or more digits.
2024-03-25 4:58 AM
I discoverd my problems nest. Its not in typecasting it is in declaration. I have few arrays named
uint16_t ADC_BUFFER_RAW [ADC_BUFFER_LENGHT];
float ADC_BUFFER [ADC_BUFFER_LENGHT];
float FFT_BUFFER [FFT_BUFFER_LENGHT];
float MAGNITUDE_BUFFER[FFT_BUFFER_LENGHT/2];
If i define FFT_BUFFER_LENGHT to be more than size of 31,
it corupts my values found in ADC_BUFFER. I have no idea why.
My .map file shows that registers are not overlaping:
.bss.fft_instance
0x00000000200002e4 0x18 ./Core/Src/main.o
0x00000000200002e4 fft_instance
.bss.ADC_BUFFER_RAW
0x00000000200002fc 0x80 ./Core/Src/main.o
0x00000000200002fc ADC_BUFFER_RAW
.bss.ADC_BUFFER
0x000000002000037c 0x100 ./Core/Src/main.o
0x000000002000037c ADC_BUFFER
.bss.FFT_BUFFER
0x000000002000047c 0x40 ./Core/Src/main.o
0x000000002000047c FFT_BUFFER
.bss.MAGNITUDE_BUFFER
0x00000000200004bc 0x20 ./Core/Src/main.o
0x00000000200004bc MAGNITUDE_BUFFER
.bss.ADC_CONVERSION_COMPLETE
0x00000000200004dc 0x1 ./Core/Src/main.o
(TEXT is slightly diferent as HTML does not support original text)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.