2024-03-19 12:01 AM - edited 2024-03-20 1:22 AM
While trying to debug a problem, it seems that another one is giving me a hard time.
One function call is not shown, another has the wrong name ("writeFLASHDoubleWord" should be "waitForBusy").
The breakpoint is also missed.
Originally the code worked, but then i moved to the new prototype. I copied the project, and made a few minor changes. Mainly just the pins.
I had some hardfault before, which happend seemingly at "CLEAR_BIT(FLASH->CR, FLASH_CR_PG);" after writing FLASH. But after seeing the above, i doubt this!
2024-03-20 7:23 AM
You can use data breakpoint (watchpoint) to find out, where does a variable get written.
JW
2024-03-20 7:25 AM - edited 2024-03-20 7:26 AM
No, the debugger wont really work with O2. The program runs fine with Og. This is quite an annoying error.
2024-03-20 7:37 AM
Likely not the issue, but using uint8_t for an index doesn't provide any efficiency
Sure the function doesn't enter twice?
2024-03-20 8:44 AM
@Tobe wrote:The value has to persist, so it has to be global.
Not true - make it static !
2024-03-20 8:47 AM
Have you tried it (data breakpoint/watchpoint) ?
The debugger still has full access to the chip's resources - it's mostly lining up source lines to executable code where the problem happens
2024-03-20 9:02 AM - edited 2024-03-20 10:10 AM
I cant think how it then would work to set breakpoints at the right places...
2024-03-20 10:37 AM
The suggestion was to set data breakpoints - ie, on the variables
2024-03-20 11:11 AM - edited 2024-03-20 11:12 AM
If the breakpoint dont "break" where they should, its not possible to debug really isnt it?
I had now printed the value of the variables:
lastBusActivityMicros = nowMicros; //TODO: DELETE VARIABLE (is not used)
inputBuffer[inputWriteIndex].timeMicros= nowMicros;
inputFrameCount++;
inputWriteIndex++;
if(inputWriteIndex >= INPUT_BUFFER_SIZE){
inputWriteIndex = 0;
inputOverFlow = true;
}
print(inputWriteIndex);
print(inputOverFlow);
}The counting of the inputWriteIndex counts as expected, and the overlow is only true, when inputWriteIndex is 1.
How in the world is this possible? Im getting crazy.
2024-03-20 11:41 AM - edited 2024-03-20 12:12 PM
2024-03-20 2:33 PM
I've just looked at the timestamps in that screenshot in the 2024-03-19 11:54 PM post, and they are consecutive.
It means, your conclusion that the index is incremented by 2 is incorrect.
What IMO happens is, that the messages are buffered in the CAN controller, and you read them out incorrectly/late/in incorrect order.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.