STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Linux STM32CubeIDE improvements - request

Hi CubeIDE developers.I use Linux Suse Tumbleweed with X11 KDE.I have only been successful in installing the Generic Linux variant of the STM32CubeIDE package.There are several annoying and time wasting things that this package does. Lets start with ...

PGump.1 by Senior III
  • 3585 Views
  • 5 replies
  • 1 kudos

Bluetooth module HC-05

I'm using STM32f411re to communicate with phone using HC-05 Bluetooth module, I want to turn an LED on, but this doesn't work when using UART2 but works well when using UART1, What could be the reason behind that?

PMato.1 by Associate II
  • 1573 Views
  • 1 replies
  • 0 kudos

Neu build Error when using STM32CubeIDE1.15.0

Version: STM32CubeIDE1.15.0 Hallo ST community,due to the project-related reason, I need to use an old compile toolchain com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.1.100.202309262110 . So I download this toolchain...

JPan.4 by Associate III
  • 1339 Views
  • 0 replies
  • 1 kudos

target is not responding issue

Hi,When I flash my code, I encounter the issue below. I have unplugged the cable of the board, but that didnt work.Could you please help me resolve ?  STMicroelectronics ST-LINK GDB server. Version 7.5.0Copyright (c) 2023, STMicroelectronics. All rig...

demir by Senior II
  • 2636 Views
  • 2 replies
  • 0 kudos

STM32CubeIDE on Windows Server 2019 for all users?

I have installed STM32CubeIDE + TouchGFX on a Windows 2019 server.It works for my account, but it does not work for other users.Question: Is it possible to install STM32CubeIDE for all users? I mean that other uses do not need to reinstall the softwa...

awiernie by Senior II
  • 979 Views
  • 0 replies
  • 0 kudos

cube-mx, xcube-ai, stm32h7 model generation.

Hello,Xcube-AI model generation. input file tflite.During model generation(Analise) i am getting error with Analyzing modelC:/Users/Yashwanth.LAPTOP-5EKATUMV/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/8.1.0/Utilities/windows/stm32ai anal...

Resolved! STM32CubeIDE build analyzer problem

Hi folks, I use latest STM32CubeIDE on Linux and noticed that build analyzer always updates "Memory Regions" tab for previous build configuration (whatever it was Debug or Release).No matter how many times I rebuild code in "Debug" configuration, the...

Lex by Associate III
  • 8439 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.