2025-03-27 1:52 PM
The CubeIDE linker doesn't seem to work properly... Any help would be greatly appreciated. ST Employee help?????
1- In the UserStartup.c, I call lv_init();
2- After compiling, it says it cannot find lv_init()
3- I see that the file lv_init.c file got compiled (lv_init() is defined in that file) - the object file was created lv_init.o
4- It seems the linker cannot find that file....
Is there a limitation on the number of files the linker can handle?
2025-03-28 12:50 PM
There are no errors in that log file and the ELF was successfully created.
Is this issue resolved?
2025-03-28 1:05 PM
Hi @TDK
I always try to get it to work even with an open question... I resolved the issue by reducing the source file sizes and removing a lot of code with #ifdefs. The full project still cannot compile, and I will send the complete project to your ticketing system later tonight.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.