2024-10-18 1:58 PM
Hello! I believe I found a code generation bug. I am currently using IDE version 1.16.1.
By default, when enabling ADC with an STM32U5, HAL_MSPInit() has the line: HAL_PWREx_EnableVddA() which is necessary to have a positive reference for the ADCs (the U5 series has some internal switch to enable VDDA)
However, when enabling the feature "Generate peripheral initialization as a pair of '.c/.h' files per peripheral", the generated code removes the VDDA Enable line from HAL_MSPInit(). This makes the same ADC code fail to start (and lead to many hours of debugging).
Hoping someone at ST can confirm this (and push a fix) to confirm the root cause!
Solved! Go to Solution.
2024-10-19 12:17 AM - edited 2025-03-06 3:24 AM
Hello @rgangwan and welcome to the ST Community :smiling_face_with_smiling_eyes:.
I confirm this code generation error, and I've escalated for correction on the future (under internal ticket number 186561).
PS: Issue solved on the last release of the STM32CubeMX
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-19 12:17 AM - edited 2025-03-06 3:24 AM
Hello @rgangwan and welcome to the ST Community :smiling_face_with_smiling_eyes:.
I confirm this code generation error, and I've escalated for correction on the future (under internal ticket number 186561).
PS: Issue solved on the last release of the STM32CubeMX
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-21 2:06 AM
Thank you for having reported.
I assume this is the exact same issue already reported to the development team and tracked by the Ticket 186561 and that will be fixed as soon as possible.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.